Write-only |
About Marker Functions |
Description |
Changes the start stimulus to the stimulus value of the marker. The stop stimulus stays the same and the span is adjusted. This command does not work with channels that are in CW or Segment Sweep mode. |
VB Syntax |
mark.SetStart |
Variable |
(Type) - Description |
mark |
A Marker (object) |
Return Type |
Not Applicable |
Default |
Not Applicable |
Examples |
mark.SetStart |
C++ Syntax |
HRESULT SetStart() |
Interface |
IMarker |