Write-only |
About Marker Functions |
Description |
Changes the stop stimulus to the stimulus value of the marker. The start stimulus stays the same and the span is adjusted. This command does not work with channels that are in CW or Segment Sweep mode. |
VB Syntax |
mark.SetStop |
Variable |
(Type) - Description |
mark |
A Marker (object) |
Return Type |
Not Applicable |
Default |
Not Applicable |
Examples |
mark.SetStop |
C++ Syntax |
HRESULT SetStop() |
Interface |
IMarker |