Write-only
About Display Formatting

ShowTable Method


Description

Shows or Hides the specified table for the window's active measurement in the lower part of the window.

 VB Syntax

win.ShowTable value

Variable

(Type) - Description

win

A NAWindow (object)

value

(enum naTable) - The table to show or hide. Choose from:

0 - naTable_None
1 - naTable_Marker
2 - naTable_Segment
3 - naTable_Limit

Return Type

Not Applicable

Default

Not Applicable

Examples

win.ShowTable naTable_limit

C++ Syntax

HRESULT ShowTable (tagNATableType table)

Interface

INAWindow