Write-only
About Display Formatting

ShowTitleBars Method


Description

Shows and Hides the Title Bars. The Title Bars are across the top of the Network Analyzer Window and each of the measurement windows. The Window name is shown in the Title Bar.

 VB Syntax

app.ShowTitleBars state

Variable

(Type) - Description

app

An Application (object)

state

(boolean)
True (1)
- Show the Title Bars
False (0)
- Hide the Title Bars

Return Type

Not Applicable

Default

Not Applicable

Examples

app.ShowTitleBars True

C++ Syntax

HRESULT ShowTitleBars/(VARIANT_BOOL bState)

Interface

IApplication