Write-only
 About Path Configurator

Store Method


Description

Saves the path configuration currently associated with channel (ch) to the specified configuration name.

This command is identical to PathConfigurationManager.StoreConfiguration Method

 VB Syntax

pathMgr.StoreConfiguration ch, name

Variable

(Type) - Description

pathMgr

PathConfigurationManager (object)

ch

(Long) Channel number of the configuration to be saved.

name

(String) Configuration name. Factory configurations can NOT be overwritten. Specifying the name of a pre-defined factory configuration will result in an error.

Return Type

Not Applicable

Default

Not Applicable

Examples

path.StoreConfiguration(2) "myMixer"

C++ Syntax

HRESULT StoreConfiguration( long channelNum, BSTR configName );

Interface

IPathConfigurationManager