Write-only |
About Cal Window |
Description |
Clears ALL flags for channels to sweep during calibration except the Cal channel. To flag a channel, see AllowChannelToSweepDuringCalAcquisition Method |
VB Syntax |
calMgr.SweepOnlyCalChannelDuringCalAcquisition |
Variable |
(Type) - Description |
calMgr |
(object) - A CalManager object |
Return Type |
Not Applicable |
Default |
Not Applicable |
Example |
calMgr.SweepOnlyCalChannelDuringCalAcquisition |
C++ Syntax |
HRESULT SweepOnlyCalChannelDuringCalAcquisition() |
Interface |
ICalManager5 |