Write-only |
About Trace Hold |
Description |
Resets the currently-stored data points to the live data trace and restarts the currently-selected Trace Hold type. |
VB Syntax |
meas.TraceHoldClear () |
Variable |
(Type) - Description |
Return Type |
Not Applicable |
Default |
Not Applicable |
Examples |
meas.TraceHoldClear |
C++ Syntax |
HRESULT TraceHoldClear( ); |
Interface |
IMeasurement16 |