Read-only

 

get_PortCData Method


Description

Reads a 4-bit value from Port C of the Aux I/O connector (pins 22-25)  and the Material Handler IO (pins 21-24 Anritsu) - (pins 22-25 Avantest).

Note: These lines are connected to both the Handler IO and Aux IO in the VNA.

 VB Syntax

value = AuxIO.get_PortCData

Variable

(Type) - Description

value

(variant) - Variable to store the returned data

AuxIO

(object) - A Hardware Auxiliary Input / Output object

Return Type

Integer

Default

None

Examples

value = auxIo.get_PortCData 'Reading a value of 15 when in Positive Logic indicates Port C lines C0, C1, C2, C3 are High. If in Negative Logic they are Low.

C++ Syntax

HRESULT get_PortCData( VARIANT* Data );

Interface

IHWAuxIO