Write-only |
About the Handler IO Connector |
Description |
Writes a TTL HI or TTL Low to output pins 3 or 4 of the Material Handler IO connector. Each pin also has a latched output which is written to with USER. With the latched (USER) outputs, the value is not applied to the associated pin until a positive edge is detected at INPUT1 (pin 2). |
VB Syntax |
handlerIo.put_Output (pin) = value |
Variable |
(Type) - Description |
handlerIo |
(object) - A HandlerIO object |
pin |
(enum as NAMatHandlerOutput) - pin to write data to. Choose from: naOutput1 - (0) - pin3 |
value |
(Variant) Value to write to the selected pin. Choose from 0 - TTL LOW 1 - TTL HIGH |
Return Type |
Not Applicable |
Default |
0 |
Examples |
handlerIo.put Output(naOutput1)= 1 |
C++ Syntax |
HRESULT put_Output ( tagNAMatHandlerOutput Output, VARIANT Data ); |
Interface |
IHWMaterialHandlerIO |