Write-only

 

put_PortCData Method


Description

Writes a 4-bit value to Port C on the Aux I/O connector (pins 22-25) and the Material Handler IO (pins 21-24 Anritsu) - (pins 22-25 Avantest).

Note: These lines are connected to both the Handler IO and Aux IO in the VNA. Therefore, this command will affect both of these connectors in the same way.

 VB Syntax

AuxIO.put_PortCData num

Variable

(Type) - Description

AuxIO

(object) - A Hardware Auxiliary Input / Output object

num

(variant) - 4 bit binary value. Choose from 0-15

Return Type

None

Default

None

Examples

HWAuxIO.put_PortCData 15  'If Positive Logic, Port C lines C0, C1, C2, C3 go High. If Negative Logic, they go Low.

C++ Syntax

HRESULT put_PortCData( VARIANT Data );

Interface

IHWAuxIO