Write-only
About the Handler IO Connector

put_Port Method


Description

Writes a value to the specified port. Use the get_Port Method to read the settings from the "readable" ports (C, D, E).

 VB Syntax

handlerIo.put_Port (port, value)

Variable

(Type) - Description

handlerIo

(object) - A HandlerIO object

port

(enum as NAMatHandlerPort) - port to put data into. Choose from:

naPortA - (0)

naPortB - (1)

naPortC - (2)

naPortD - (3)

naPortE - (4)

naPortF - (5)

naPortG - (6)

naPortH - (7)

value

The number of the data bits to set. The following table shows what the value represents:

Note: When writing to port G, port C must be set to output mode
When writing to port H, both port C and port D must be set to output mode. Use Port Mode Property

 

Port

Max allowable <num>

MSB...........................................LSB
23...................................................0

 

 

A

255

A7...A0

Write-only

 

B

255

B7...B0

Write-only

 

C

15

C3...C0

Read-Write

 

D

15

D3...D0

Read-Write

 

E

255

D3...D0 + C3...C0

Read-Write

 

F

65535

B7...B0 + A7...A0

Write-only

 

G

1048575

C3...C0 + B7...B0 + A7...A0

Write-only

 

H

16777215

D3...D0 + C3...C0 + B7...B0 + A7...A0

Write-only
 

Return Type

Not Applicable

Default

Not Applicable

Examples

handlerIo.put_Port(naPortB, 1)

C++ Syntax

HRESULT put_Port ( tagNAMatHandlerPort Port, VARIANT Data );

Interface

IHWMaterialHandlerIO