Write-only |
About Source Power Cal |
Description |
Inputs source power calibration data (as variant data type) to this channel for a specific source port. Note: This method is Superseded. It is replaced by PutSourcePowerCalDataEx Method |
VB Syntax |
chan.putSourcePowerCalData sourcePort, data |
Variable |
(Type) - Description |
chan |
(object) – A Channel object |
sourcePort |
(long integer) – The source port for which calibration data is being requested. |
data |
(variant) – Array of source power cal data being input. |
Return Type |
None |
Default |
Not Applicable |
Examples |
chan.putSourcePowerCalData 1, varData |
C++ Syntax |
HRESULT putSourcePowerCalData(long sourcePort, VARIANT varData); |
Interface |
IChannel |