InterfaceControl Object


Description

Contains the methods and properties that support Interface Control.

Accessing the InterfaceControl object

Dim app As AgilentPNA835x.Application
Set app = CreateObject("AgilentPNA835x.Application", <analyzerName>)

Dim IntControl As InterfaceControl
Set IntControl = app.InterfaceControl

See Also:

 

Methods

Interface

Description

 

 

 

Properties

 

Description

ConfigurationFile

InterfaceControl

Recalls an Interface Control file

State

InterfaceControl

Turns Interface Control ON and OFF

 

InterfaceControl History

Interface

Introduced with VNA Rev:

InterfaceControl

5.2