| Write/Read | About ADC Multiple Recordings | 
| Description | Set and read the ON/OFF state of the multiple recording function. Multiple recording allows the ADC Record Size to be divided and acquired in smaller "chunks" and also to specify a wait period between these acquisitions. | 
| VB Syntax | sa.ADCMultRecState = value | 
| Variable | (Type) - Description | 
| sa | A SpectrumAnalyzer (object) | 
| value | (Boolean) Choose from: 0 - OFF - ADC record size "chunking" OFF. 1 - ON - ADC record size "chunking" ON. | 
| Return Type | Boolean | 
| Default | 0 | 
| Examples | sa.ADCMultRecState = OFF Write | 
| value = sa.ADCMultRecState 'Read | |
| C++ Syntax | HRESULT put_ADCMultRecState(VARIANT_BOOL bEnable); HRESULT get_ADCMultRecState(VARIANT_BOOL* bEnable); | 
| Interface | ISpectrumAnalyzer |