Write/Read
About SA Application

EnableADCSampleRateAuto Property


Description

Set and read how the ADC sample rate is set. When set to 1, ADC sample rate is set based on the ADC filter setting.

VB Syntax

sa.EnableADCSampleRateAuto = value

Variable

(Type) - Description

sa

A SpectrumAnalyzer (object)

value

(Boolean) Choose from:

0 - OFF - ADC sampling rate is set manually using ADCSampleRate.

1 - ON - Automatically select ADC sample rate based on the ADC filter setting.

Learn about these settings.

Return Type

Boolean

Default

1

Examples

sa.EnableADCSampleRateAuto = 1  'Write

value = sa.EnableADCSampleRateAuto 'Read

See an example program.

C++ Syntax

HRESULT put_EnableADCSampleRateAuto(VARIANT_BOOL bEnable);

HRESULT get_EnableADCSampleRateAuto(VARIANT_BOOL* bEnable);

Interface

ISpectrumAnalyzer