Write/Read | 
About External DC Devices | 
Description | 
 Sets and returns the Abort Sweep command for an external DC Source and an external DC Meter.  | 
VB Syntax | 
 extDC.AbortSweepCmd = value  | 
Variable | 
(Type) - Description | 
| 
 extDC  | 
 A ExternalDCDevice (object)  | 
| 
 value  | 
 (String) The SCPI command used to abort or reset the DC Source or DC Meter.  | 
Return Type | 
 String  | 
Default | 
 " " Empty String  | 
Examples | 
 extDC.AbortSweepCmd = "ABORt" 'Write value = extDC.AbortSweepCmd 'Read  | 
C++ Syntax | 
 HRESULT get_AbortSweepCmd( BSTR* cmd); HRESULT put_AbortSweepCmd( BSTR cmd);  | 
Interface | 
 IExternalDCDevice3  |