Write/Read
About Trigger

AcceptTriggerBeforeArmed Property


Description

Determines what happens to an EDGE trigger signal if it occurs before the VNA is ready to be triggered. (LEVEL trigger signals are always ignored.)  For more information, see External triggering.

 VB Syntax

trigsetup.AcceptTriggerBeforeArmed = boolean

Variable

(Type) - Description

trigsetup

A TriggerSetup2 (object)

boolean

Choose from:

False - A trigger signal is ignored if it occurs before the VNA is ready to be triggered.

True - A trigger signal is remembered and then used when the VNA becomes armed (ready to be triggered). The VNA remembers only one trigger signal.

Return Type

Boolean

Default

False

Examples

trigsetup.AcceptTriggerBeforeArmed = True 'Write

 

C++ Syntax

HRESULT get_AcceptTriggerBeforeArmed( BOOL *pVal);

HRESULT put_AcceptTriggerBeforeArmed( BOOL newVal);

Interface

ITriggerSetup2