Read / Write
About Performing a Calibration

AcquisitionDirection Property


Description

Specifies the direction of each part of a 2-port calibration.

 VB Syntax

cal.AcquisitionDirection = value

Variable

(Type) - Description

cal

A Calibrator (object)

value

(enum NADirection) - Choose from:

0 - naForward - measures the forward direction
1 - naReverse
- measures the reverse direction

Return Type

Long Integer

Default

naForward

Examples

cal.AcquisitionDirection = naForward

C++ Syntax

HRESULT AcquisitionDirection(tagNADirection dir);

Interface

ICalibrator