Write/Read
About Compression Mode

AcquisitionMode Property


Description

Set and read the method by which gain compression data is acquired.

 VB Syntax

gca.AcquisitionMode = value

Variable

(Type) - Description

gca

A GainCompression (object)

value

(NAGCAAcquisitionMode)  Choose from:

  • naSmartSweep (0)  Iterate quickly to find compression point

  • naSweepPowerAtEachFreq2D (1)  Sweep power at each frequency

  • naSweepFreqAtEachPower2D (2) Sweep frequency at each power level

Return Type

Enum

Default

naSmartSweep

Examples

gca.AcquisitionMode = naSmartSweep 'Write

acqMode = gca.AcquisitionMode 'Read

C++ Syntax

HRESULT get_AcquisitionMode(tagNAGCAAcquisitionMode* mode)

HRESULT put_AcquisitionMode(tagNAGCAAcquisitionMode mode)

Interface

IGainCompression