Read-Only
About Acquisition Time

AcquisitionTime Property


Description

Returns the LO acquisition time which is the ADC Record Size x ADC Sampling Frequency (10 nsec or 40 nsec) x (1 + Stacking) x (Video Average.Coefficient).

VB Syntax

value = sa.AcquisitionTime

Variable

(Type) - Description

sa

A SpectrumAnalyzer (object)

value

(Double) Variable to store the returned number of LOs.

Learn about these settings.

Return Type

Double

Default

N/A

Examples

value = sa.AcquisitionTime 'Read

See an example program.

C++ Syntax

HRESULT get_AcquisitionTime(double* val);

Interface

ISpectrumAnalyzer