Read-only
About Markers

ActiveMarker Property


Description

Returns a handle to the Active Marker object. You can either (1) use the handle directly to access Marker properties and methods, or (2) set a variable to the Marker object. The variable retains a handle to the original object if another Marker becomes active.

 VB Syntax

1) meas.ActiveMarker.<setting>
or

2) Set
mark = meas.ActiveMarker

Variable

(Type) - Description

meas

(object) - An Measurement object

<setting>

A marker property (or method) and arguments

mark

(object) - A marker object

Return Type

marker object

Default

None

Examples

Public mark as marker
Set mark = meas.ActiveMarker

C++ Syntax

HRESULT get_ActiveMarker(IMarker** marker)

Interface

IMeasurement