Read-only |
About Calibration Kits |
Description |
Returns a handle to the Active CalKit object. The active cal kit is the kit selected for use in Unguided calibrations. You can either (1) use the handle directly to access CalKit properties and methods, or (2) set a variable to the CalKit object. The variable retains a handle to the original object if another CalKit becomes active. |
VB Syntax |
1) app.ActiveCalKit.<setting> |
Variable |
(Type) - Description |
app |
An Application (object) |
<setting> |
A CalKit property (or method) and arguments |
cKit |
(object) - A CalKit object |
Return Type |
CalKit object |
Default |
None |
Examples |
Public cKit as calKit |
C++ Syntax |
HRESULT get_ActiveCalKit (ICalkit * kit) |
Interface |
IApplication |