Write/Read
About GCA Analysis

AnalysisIsDiscreteFreq Property


Description

Sets and returns whether the CW frequency for the compression analysis trace can be set to only the discrete frequencies or provides interpolation.

 VB Syntax

gcaMeas.AnalysisIsDiscreteFreq = value

Variable

(Type) - Description

gcaMeas

A GainCompressionMeas (object)

value

(Boolean)  Choose from:

False - Interpolated data points.

True - Discrete data points only.

Return Type

Boolean

Default

False

Examples

gcaMeas.AnalysisIsDiscreteFreq = True 'Write

isDisc = gca.AnalysisIsDiscreteFreq 'Read

C++ Syntax

HRESULT get_AnalysisIsDiscreteFreq(VARIANT_BOOL* value)

HRESULT put_AnalysisIsDiscreteFreq(VARIANT_BOOL  value)

Interface

IGainCompressionMeas