Read only
About Measurement Classes

AvailableMeasurementClasses Property


Description

Returns a list of available measurement classes on the VNA.

 VB Syntax

value = cap.AvailableMeasurementClasses

Variable

(Type) - Description

value

(Variant) - Variable to store the returned list of measurement classes.

cap

A Capabilities (object)

Return Type

Variant

Default

Not Applicable

Examples

'Read all measurement classes

Set app = CreateObject("AgilentPNA835x.Application")

Set cap = app.Capabilities

meas=cap.AvailableMeasurementClasses

dim i

For i = 0 To UBound(meas)

 msg = msg & meas(i) & vbCrLf

Next

MsgBox msg  

C++ Syntax

HRESULT get_AvailableMeasurementClasses(Variant *value);

Interface

ICapabilities7