Read-only
About PNOP Marker Search

BackOffPout Property


Description

Returns the BackOffPout result of the PNOP marker search.

PBO Out =  Marker 2 Y-axis

 VB Syntax

bOffPout = pnop.BackOffPout

Variable

(Type) - Description

bOffPout

(double) - Variable to store returned value

pnop

A PNOP (object)

Return Type

Double

Default

Not applicable

Examples

bOffPout = pnop.BackOffPout 'Read

See example program

C++ Syntax

HRESULT get_BackOffPout(double* pNewVal)

Interface

IPNOP