Write/Read
About iTMSA

BalancedPortTrueState(bpnum) Property


Description

Sets and reads the True Mode state for a specified balanced port.

 VB Syntax

balStim.BalancedPortTrueState(bpnum)  = value

Variable

(Type) - Description

balStim

A BalancedStimulus (object)

bpnum

Balanced port number. This corresponds to the Balanced Port number in the GUI.

value

(Boolean) Choose from:

ON or 1   Turns True Mode ON.

OFF or 0  Turns True Mode OFF.

Return Type

Boolean

Default

False

Examples

balStim.BalancedPortTrueState(2) = ON   'Write

var = balStim.BalancedPortTrueState(2)   'Read

C++ Syntax

HRESULT get_BalancedPortTrueState (int bpnum, VARIANT_BOOL *pState)

HRESULT put_BalancedPortTrueState (int bpnum, VARIANT_BOOL pState)

Interface

IBalancedStimulus3