Write/Read
About Spectrum Analyzer Markers

BandDensityACPRState Property


Description

Sets and reads the ACPR density marker.

 VB Syntax

mkr.BandDensityACPRState = value

Variable

(Type) - Description

mkr

A Marker (object)

value

(Enum as NAStates) Choose from:

naOFF (or 0) - Turn ACPR density marker OFF

naON (or 1) - Turn ACPR density marker ON

Return Type

Boolean

Default

naOFF

Examples

mkr.BandDensityACPRState = 0   Write

value = mkr.BandDensityACPRState 'Read

C++ Syntax

HRESULT get_BandDensityACPRState(tagNAStates* pState)

HRESULT put_BandDensityACPRState(tagNAStates pState)

Interface

IMarker9