Write/Read
About Spectrum Analyzer Markers

BandDensityEQSPan Property


Description

Sets and reads the frequency span used by Power Density to normalize the power.

 VB Syntax

mkr.BandDensityEQSPan = value

Variable

(Type) - Description

mkr

A Marker (object)

value

(Double) Choose a span

Return Type

Double

Default

1 MHz

Examples

mkr.BandDensityEQSPan = 1e6   'Write

value = mkr.BandDensityEQSPan  'Read

C++ Syntax

HRESULT get_BandDensityEQSPan(double* pVal)

HRESULT put_BandDensityEQSPan(double newVal)

Interface

IMarker8