Write/Read
About Spectrum Analyzer Markers

BandDensityNPRState Property


Description

Sets and reads the NPR density marker.

 VB Syntax

mkr.BandDensityNPRState = value

Variable

(Type) - Description

mkr

A Marker (object)

value

(Enum as NAStates) Choose from:

naOFF (or 0) - Turn NPR density marker OFF

naON (or 1) - Turn NPR density marker ON

Return Type

Boolean

Default

naOFF

Examples

mkr.BandDensityNPRState = 0   Write

value = mkr.BandDensityNPRState 'Read

C++ Syntax

HRESULT get_BandDensityNPRState(tagNAStates* pState)

HRESULT put_BandDensityNPRState(tagNAStates pState)

Interface

IMarker9