Write/Read |
About Spectrum Analyzer Markers |
Description |
Sets and reads the band power density bandwidth. |
VB Syntax |
mkr.BandDensityPowerBW = value |
Variable |
(Type) - Description |
mkr |
A Marker (object) |
value |
(Double) Choose a bandwidth |
Return Type |
Double |
Default |
1 MHz |
Examples |
mkr.BandDensityPowerBW = 1e6 'Write value = mkr.BandDensityPowerBW 'Read |
C++ Syntax |
HRESULT get_BandDensityPowerBW(double* pVal) HRESULT put_BandDensityPowerBW(double newVal) |
Interface |
IMarker8 |