Write/Read
About Spectrum Analyzer Markers

BandDensityPowerState Property


Description

Sets and reads the band power density state.

 VB Syntax

mkr.BandDensityPowerState = value

Variable

(Type) - Description

mkr

A Marker (object)

value

(Enum as NAStates) Choose from:

naOFF (or 0) - Turn band power density marker OFF

naON (or 1) - Turn band power density marker ON

Return Type

Boolean

Default

naOFF

Examples

mkr.BandDensityPowerState = 0   Write

value = mkr.BandDensityPowerState 'Read

C++ Syntax

HRESULT get_BandDensityPowerState(tagNAStates* pState)

HRESULT put_BandDensityPowerState(tagNAStates pState)

Interface

IMarker8