Write/Read |
About Spectrum Analyzer Markers |
Description |
Sets and reads the band tone density state. |
VB Syntax |
mkr.BandDensityToneState = value |
Variable |
(Type) - Description |
mkr |
A Marker (object) |
value |
(Enum as NAStates) Choose from: naOFF (or 0) - Turn band tone density marker OFF naON (or 1) - Turn band tone density marker ON |
Return Type |
Boolean |
Default |
naOFF |
Examples |
mkr.BandDensityToneState = 0 Write value = mkr.BandDensityToneState 'Read |
C++ Syntax |
HRESULT get_BandDensityToneState(tagNAStates* pState) HRESULT put_BandDensityToneState(tagNAStates pState) |
Interface |
IMarker8 |