Write/Read
About Marker Search

BandwidthSearch Property


Description

Sets the bandwidth search preference to start a bandwidth or notch search in either peak or marker mode.

 VB Syntax

pref.BandwidthSearch = value

Variable

(Type) - Description

pref

A Preferences (object)

value

(Enum) - Choose from:

0 - searchPeak - Search starts at the maximum y-value of the full sweep of data.

1 - searchMarker - Search starts at the x and y position of the active marker.

Return Type

Enum

Default

searchPeak

Examples

pref.BandwidthSearch = 1 'Write

bwsearchmode = pref.BandwidthSearch 'Read

C++ Syntax

HRESULT put_BandwidthSearch(enum BandwidthSearchMode preference)
HRESULT get_BandwidthTarget(enum BandwidthSearchMode* preference)

Interface

IPreferences18