| Write/Read | About SA Application | 
| Description | Set and read the maximum value for wide DFT bandwidth. The maximum wide DFT bandwidth setting is 44 MHz. The AutoBandwidth must be set to OFF to set this value manually. | 
| VB Syntax | sa.dft.BandwidthWideMax = value | 
| Variable | (Type) - Description | 
| sa.dft | A SpectrumAnalyzerDFT (object) | 
| Return Type | Double | 
| Examples | sa.dft.BandwidthWideMax = 44e6 'Write | 
| value = sa.dft.BandwidthWideMax 'Read | |
| C++ Syntax | HRESULT put_BandwidthWideMax(double maxbw); HRESULT get_BandwidthWideMax(double* maxbw); | 
| Interface | ISpectrumAnalyzerDFT |