Write/Read |
About SA Application |
Description |
Set and read the minimum value for wide DFT bandwidth. The minimum wide DFT bandwidth setting is 500 kHz. The AutoBandwidth must be set to OFF to set this value manually. |
VB Syntax |
sa.dft.BandwidthWideMin = value |
Variable |
(Type) - Description |
|
sa.dft |
A SpectrumAnalyzerDFT (object) |
Return Type |
Double |
Examples |
sa.dft.BandwidthWideMin = 5e5 'Write |
|
value = sa.dft.BandwidthWideMin 'Read |
|
C++ Syntax |
HRESULT put_BandwidthWideMin(double minbw); HRESULT get_BandwidthWideMin(double* minbw); |
Interface |
ISpectrumAnalyzerDFT |