Write/Read
About Limits

BeginStimulus Property


Description

When constructing a limit line, specifies the beginning X-axis value.

 VB Syntax

limtseg.BeginStimulus = value

Variable

(Type) - Description

limtseg

A LimitSegment (object)

value

(double) - Stimulus value. No units

Return Type

Double

Default

0

Examples

Set limtseg = meas.LimitTest(1)
 limtseg.Type = naLimitSegmentType_Maximum
 limtseg.BeginStimulus = 3e9
 limtseg.EndStimulus = 4e9
 limtseg.BeginResponse = 10
 limtseg.EndResponse = 10

BegStim = limtseg.BeginStimulus 'Read

C++ Syntax

HRESULT get_BeginStimulus(double *pVal)
HRESULT put_BeginStimulus(double newVal)

Interface

ILimitSegment