| Write/Read | About SA Application | 
| Description | Enables/disables binary file (*.bin) output. | 
| VB Syntax | sa.dft.BinaryFileEnabled = value | 
| Variable | (Type) - Description | 
| sa.dft | A SpectrumAnalyzerDFT (object) | 
| value | (Boolean) Choose from: 0 - OFF - Disable binary file output. 1 - ON - Enable binary file output. | 
| Return Type | Boolean | 
| Default | OFF | 
| Examples | sa.dft.BinaryFileEnabled = ON 'Write | 
| value = sa.dft.BinaryFileEnabled 'Read | |
| C++ Syntax | HRESULT get_BinaryFileEnabled(VARIANT_BOOL* enable) | 
| Interface | ISpectrumAnalyzerDFT |