Read/Write
About Dynamic Uncertainty

CableRepeatabilityEnabled Property


Description

Sets and returns the ON/OFF state of allowing cable repeatability data to contribute to the uncertainty of a calibration performed using Dynamic Uncertainty. Repeatability data must also be present for the ports at the time the calibration is performed.

VB Syntax

uncertMan.CableRepeatabilityEnabled = value

Variable

(Type) - Description

uncertMan

An UncertaintyManager Object

value

(Boolean) Enable state. Choose from:

True - Cable repeatability uncertainty ON.

False - Cable repeatability uncertainty OFF.

Return Type

Boolean

Default

True

Examples

uncertMan.CableRepeatabilityEnabled = True

See example program

C++ Syntax

HRESULT get_CableRepeatabilityEnabled([out,retval] VARIANT_BOOL* pState);

HRESULT put_CableRepeatabilityEnabled([in] VARIANT_BOOL state);

Interface

IUncertaintyManager