Read / Write
 

CalibrationPort Property - Obsolete


Description

Note: Beginning with Rev 6.0, this command is no longer necessary. Because of improved calibration techniques, Both is always selected although a power meter measurement is performed only on port 1.

Specifies which SMC port to calibrate.

VB Syntax

SMC.CalibrationPort = value

Variable

(Type) - Description

SMC

SMCType (object)

value

(String) Port number to be calibrated. Choose from:

  • 1 - SMC forward

  • 2 - SMC reverse

  • Both

Return Type

String

Default

1

Examples

value = SMC.CalibrationPort = "Both"

C++ Syntax

HRESULT put_CalibrationPort(BSTR port);

HRESULT get_CalibrationPort(BSTR *port);

Interface

SMCType

VMCType