Write/Read
About Gating

Center Property


Description

Sets or returns the Center time of either Gating or Time Domain transform windows

 VB Syntax

object.Center = value

Variable

(Type) - Description

object

(object) As Gating
or

(object)
As Transform

value

(double) - Center time in seconds. Choose any number between:
 ± (points-1) / frequency span

Return Type

Double

Default

0

Examples

trans.Center = 4.5e-9 'sets the Center time of a transform window -Write
gate.Center = 4.5e-9 'sets the Center time of a gating window -Write

cnt = trans.Center 'Read

C++ Syntax

HRESULT get_Center(double *pVal)
HRESULT put_Center(double newVal)

Interface

ITransform
IGating