Write/Read |
About External SMU Devices |
Description |
Set and return the state of activation of the SMU device. |
VB Syntax |
extSMU.ChanActive <chanNum>,<value> |
Variable |
(Type) - Description |
extSMU |
An ExteranlSMUDevice (object) |
<chanNum> |
Channel number for the external SMU |
<value> |
(Boolean) Choose from: True - Channel is active. False - Channel is NOT active. |
Return Type |
Boolean |
Default |
Not applicable |
Examples |
extSMU.ChanActive = 2,True 'Write |
C++ Syntax |
HRESULT get_ChanActive( long chanNum, VARIANT_BOOL* value) HRESULT put_ChanActive( long chanNum, VARIANT_BOOL value) |
Interface |
IExternalSMUDevice |