Read-only
About Cal Sets

ChannelClients Property


Description

Returns the numbers of the channels using the calset.

VB Syntax

value = calSet.ChannelClients

Variable

(Type) - Description

calSet

A CalSet (object)

Return Type

1-dimensional variant array

Default

Not Applicable

Examples

Set app = CreateObject("AgilentPNA835x.Application")

Set calset = app.GetCalManager.CalSets.Item(2)

arry = CalSet.ChannelClients

For i = 0 to UBound(arry)

  Msgbox (arry(i))

Next

C++ Syntax

HRESULT get_ChannelClients (VARIANT* vals)

Interface

ICalSet8