Description |
Specifies the direction in which to characterize the calibration mixer. Learn more about the calibration mixer. |
VB Syntax |
VMC.CharMixerReverse = bool |
Variable |
(Type) - Description |
VMC |
VMCType (object) |
bool |
(Boolean) 0 - Characterize the calibration mixer in the SAME direction as that specified in the mixer setup. 1 - Characterize the calibration mixer in the REVERSE direction as that specified in the mixer setup. |
Return Type |
Boolean |
Default |
0 |
Examples |
VMC.CharMixerReverse = 0 |
C++ Syntax |
HRESULT put_CharMixerReverse(VARIANT_BOOL bcharReverse); HRESULT get_CharMixerReverse(VARIANT_BOOL *bcharReverse); |
Interface |
VMCType2 |