Read/Write
About CharacterizeMixer

CharacterizeMixerOnly Property


Description

Sets and returns whether to perform ONLY a mixer characterization.

VB Syntax

VMC.CharacterizeMixerOnly = bool

Variable

(Type) - Description

VMC

VMCType (object)

bool

(Boolean)

True - Perform ONLY mixer characterization.

False - Perform both mixer characterization and calibration.

Return Type

Boolean

Default

False

Examples

value = VMC.CharacterizeMixerOnly

C++ Syntax

HRESULT put_CharacterizeMixerOnly(VARIANT_BOOL bCharMixerOnly);

HRESULT get_CharacterizeMixerOnly(VARIANT_BOOL *bCharMixerOnly);

Interface

VMCType