Write/Read
About Gain Compression

CompressionBackoff Property


Description

Set and read value for the BackOff compression algorithm.

 VB Syntax

gca.CompressionBackoff = value

Variable

(Type) - Description

gca

A GainCompression (object)

value

(Double)  Backoff value in dB. Choose from 30 to (-30)

Return Type

Double

Default

10

Examples

gca.CompressionBackoff = 7 'Write

acqMode = gca.CompressionBackoff 'Read

C++ Syntax

HRESULT get_CompressionBackoff(double* pValue)

HRESULT put_CompressionBackoff(double newValue)

Interface

IGainCompression