Write/Read |
About Gain Compression |
Description |
Set and read the desired gain reduction (from reference gain). This value is used for Compression Methods: Compression from Linear Gain and Compression from Maximum Gain. |
VB Syntax |
gca.CompressionLevel = value |
Variable |
(Type) - Description |
gca |
A GainCompression (object) |
value |
(Double) - Compression level in dB. Choose a value greater than 0.1 dB. |
Return Type |
Double |
Default |
1 |
Examples |
gca.CompressionLevel = 1.5 'Write |
compLevel = gca.CompressionLevel 'Read |
|
C++ Syntax |
HRESULT get_CompressionLevel(double* pVal) HRESULT put_CompressionLevel(double newVal) |
Interface |
IGainCompression |