Write/Read
About Ext DC Devices

DCCorrection Property


Description

Sets and returns the correction ON/OFF state for a DC Meter and a DC Source.

 VB Syntax

extDC.DCCorrection = value

Variable

(Type) - Description

extDC

An ExternalDCDevice (object)

value

(Boolean) Correction ON/OFF state. Choose from:

True - Turn Correction ON

False - Turn Correction OFF

Return Type

Boolean

Default

False

Examples

extDC.DCCorrection = True 'Write

bool = extDC.DCCorrection 'Read

C++ Syntax

HRESULT get_DCCorrection (BOOL *pValue)

HRESULT put_DCCorrection (BOOL newVal)

Interface

IExternalDCDevice