Write/Read |
Description |
Set and read the order for the specified DC source in the multi-dimensional sweep. |
VB Syntax |
md.DCOrder (name,port) = value |
Variable |
(Type) - Description |
md |
A MultiDimensionalSweep (object) which belongs to a SA channel. |
name,port |
(string) Name of the "DC source, port" |
value |
(long) Dimension order. Choose an integer value of 1 or higher. |
Return Type |
long |
Default |
1 |
Examples |
md.DCOrder ("AO1") = 2 'Write |
value = md.DCOrder("MyDCSource,Port 1") 'Read |
|
C++ Syntax |
HRESULT put_DCOrder (BSTR name, long value); HRESULT get_DCOrder (BSTR name, long* value); |
Interface |
IMultiDimensionalSweep |