Write/Read | 
About SA Application | 
Description | 
 Set and read the ON/OFF state of the DC sources. If ON, the DC sources sweep between their start and stop voltages.  | 
VB Syntax | 
 sa.DCSourceSweepState = value  | 
Variable | 
(Type) - Description | 
| 
 sa  | 
 A SpectrumAnalyzer (object)  | 
| 
 value  | 
 (Boolean) Choose from: 0 - OFF - DC sweep OFF. 1 - ON - DC sweep ON.  | 
Return Type | 
 Boolean  | 
Default | 
 0  | 
Examples | 
 sa.DCSourceSweepState = OFF Write  | 
| 
 value = sa.DCSourceSweepState 'Read  | 
|
C++ Syntax | 
 HRESULT put_DCSourceSweepState(VARIANT_BOOL bEnable); HRESULT get_DCSourceSweepState(VARIANT_BOOL* bEnable);  | 
Interface | 
 ISpectrumAnalyzer  |