Write / Read |
About Display Colors |
Description |
Set and return the color of Data and Limit Lines for nth trace in a window. |
VB Syntax |
trace(n).DataAndLimits = value |
Variable |
(Type) - Description |
trace(n) |
One of the 8 ComTraceColors objects |
value |
(Long Integer) - RGB color of the DataAndLimits pen. Convert the three RGB colors to an integer as follows: RGB = R+(G*2^8)+(B*2^16) To find the three RGB values from the Display Colors dialog, click Change Color, then Define Custom Color. |
Return Type |
Long |
Default |
Varies for each trace. |
Examples |
R = 10 |
C++ Syntax |
HRESULT get_DataAndLimits(long* pVal); HRESULT put_DataAndLimits(long newVal); |
Interface |
ITraceColors |